Command 'Edge Detection'Permalink

Symbol FBD:_cds_icon_edge_detection_fup, symbol LD:_cds_icon_edge_detection_kop, shortcut: [Ctrl] + [E]

Function: This command inserts an edge detector before the selected box input or box output.

Call: Main menu “FBD/LD/IL”, context menu

Requirements: The FBD or LD editor is active. A box input or box output is selected.

See also