Function: The command opens the default dialog for saving a file to the local file system.
The filter is set to CSV file format. After specifying a name and storage location, CODESYS saves the I/O mapping configuration in a CSV file with the delimiter which was defined as the list
separator (comma or semicolon) in the regional settings in Windows.
Call: Context menu of a device object in the “Devices” view
Requirement: A device object with an I/O mapping configuration is selected in the device tree.
Parameter names which are not unique are numbered incrementally @<n> in this file.
For more information, see: ⮫ “Configuring Devices and I/O Mapping ”, ⮫ “Linking a device input with an existing project variable ("mapping") ”, ⮫ “Mapping a device input to a recently created project variable ”, ⮫ “Linking a device with a function block instance ”, ⮫ “Changing and fixing an address value in the I/O map ”, ⮫ “Configuration of the I/O variable update ”, ⮫ “Monitoring of variables in the I/O map in online mode ”, ⮫ “Generating implicit variables for the forcing of I/Os ”, ⮫ “I/O mapping in one dialog for multiple devices ”