Function: This command opens a dialog box for exporting objects from a project to an XML file.
Call: Menu bar: “Project”.
Dialog 'Export'
This dialog box lists all objects from the device tree, POU tree, and module tree that CODESYS can export.
|
One file per subtree |
|
|
“Saved version” |
This version should correspond to the target version where the export file will later be imported. If the current project contains plug-ins or add-ons that are not available in the selected memory format (profile), then the “Extend Profile” dialog box opens. In this dialog box, the selected profile can be extended with the add-ons. |
See also
:
: