Symbol:
Function: The dialog contains options for compiling (build operation) the object.
Call: “View Properties” command; context menu of the object in the device tree
Name |
Description |
---|---|
“Exclude from build” |
The object entry is displayed in green fonts in the “Devices” view or in the “POUs” view. |
“External implementation” “(Late link in the runtime system)” |
The object name is appended with |
“Enable system call” |
Background: Different from CODESYS V2.3 Gateway Server, the ADR operator in V3 can be used with function names, program names, function block names, and method
names. It replaces the BUT: It is not possible to call function pointers from within CODESYS. |
“Link always” |
Note: The pragma |
“Compiler defines” |
Here you can specify "defines" or conditions for compiling the object (conditional
compile). You can also specify the Example: |
“Additional compiler definitions from the device description” |
|
“Defined in device” |
List of compiler definitions which originate from the device description These compiler definitions are used in the build if they are not listed in the “Ignored definitions” field. |
“Ignored definitions” |
List of compiler definitions from the device description which are not used in the build |
Copies the selected compiler definition from the “Defined in device” field to the “Ignored definitions” field |
|
Moves the selected compiler definition from the “Ignored definitions” field to the “Defined in device” field The compiler definition is used in the build. |
For more information, see: ⮫ “Conditional Pragmas ”, ⮫ Further information
-
See also: ⮫ {attribute 'linkalways'}