Here, an existing breakpoint or data breakpoint can be converted into an execution point.
“Execution point (execution does not stop at breakpoint)” |
|
“Execute the following code” |
Code which is executed when the execution point is reached Looping structures (For, While) and IF or CASE expressions are not possible. |
“Print a message in the device log” |
This option is available only when you select the “Enable logging in breakpoints” option in “Project Settings Compile options”. CODESYS can output variables with the |