Command 'Display Mode' - 'Binary', 'Decimal', 'Hexadecimal'Permalink

Function: These commands in the “Display Mode” submenu are used for setting the format of values in the display mode when monitoring in online mode.

Call: Main menu “Debug”.

Requirement: The project is in either online or offline mode.

The "Binary" and "Hexadecimal" display modes are unsigned, and "Decimal" is signed.

See also