Function: This command collapses all expanded code segments in the textual editor or result locations in the cross-reference list. In this way, only the uppermost level of code and only the root node of the result locations displayed.
Requirement: A textual editor is active and indentation is activated in the “Options” (“Text Editor” category); or the cross-reference list is active.
Call: In textual editors: main menu “Edit Advanced”, or right-click. In the cross-reference list: right-click.
See also