Function: The command deletes the compile information for all applications in the project.
Call: “Build” menu
During the last download, the compile information was created in the local file system and saved to a file (*.compileinfo).
The command requires a download before a new login. An online change is no longer possible. Different from the “Clean” command (only of the active application), CODESYS again generates the language model for all objects, which is very time-consuming.




NOTICE

Reconsider carefully whether or not executing the command is really necessary. If you only want to rebuild and download the active application, then execute the “Clean” command.