Command: Set Execution Order Permalink

Function: The command opens a dialog for setting the number of the selected element to any value.

Call: “CFC → Execution Order” menu, “Execution Order” in the context menu

Requirements: A CFC editor is active and the “Explicit Execution Order Mode” property is selected. Exactly one element is selected.

The selected element gets the number specified in the dialog. The remaining elements are numbered so that their execution order remains the same. The topological positions of the elements are retained anyway.