Command: Send to Front Permalink

Symbol: cfc_icon_send_to_front.png

Function: The command numbers the elements so that the selected elements are located at the front of the execution order.

Call: “CFC  Execution Order” menu, “Execution Order” in the context menu

Requirements: A CFC editor is active and the “Explicit Execution Order Mode” property is selected. At least one element is selected.

The selected elements get the lowest numbers beginning at 0 while keeping the previous order. The remaining elements are numbered so that their execution order remains the same. The topological positions of the elements are retained anyway.