Command: Route All Connections Permalink

Symbol: cfc_icon_route_all_connections.png

Function: The command undoes all manual changes to the connections in the program and restores the original state.

Call: “CFC  Routing” menu, “Routing” in the context menu

Requirement: A CFC editor is active.

Connections which are fixed with control points cannot be automatically routed. As a result, you have to remove the control points before executing the command. To do this, click “Remove Control Point”.

Furthermore, for manually changed connections marked with the cfc_icon_unreleased_connection.png icon, you have to click “Unlock Connection”.