Symbol:
, [Ctrl]+[U]
Function: The command restores the deleted pins of a box. If the layout of the inputs or outputs of an instance differs from the declaration of the function block, then the command refreshes the layout of the inputs and outputs of the instance according to the declaration.
Call: “CFC Pins” menu; “Pins” in the context menu
Requirements: A CFC editor is active and a box is selected.
The command restores all inputs and outputs and their box layout as they are defined in their implementation.
See also