Command: Move Down Permalink

Symbol: cfc_icon_move_down.png

Function: The command numbers the elements so that the selected elements are located one position backward.

Call: “CFC → Execution Order” menu, “Execution Order” in the context menu

Requirements: A CFC editor is active and at least one element is selected. The “Explicit Execution Order Mode” property is selected.

The selected elements get a numbering increased by one while keeping the previous order. The elements are processed one position later. The remaining elements are numbered so that their execution order remains the same. The topological positions of the elements are retained anyway.