Command: EN/ENO Permalink

Symbol: cfc_icon_enenq.png

Function: The command adds a Boolean input “EN” (Enable) and a Boolean output “ENO” (Enable Out) to the selected box.

Call: “CFC” menu; context menu

Requirement: A CFC editor is active. A box is selected.

The added “EN” input activates the box. The box is executed only if the value is ‎TRUE‎. The value of this signal is output at “ENO” output.