Command: Edit Page Size Permalink

Function: The command opens the “Edit Page Size” dialog. There you change the size of the page-oriented CFC editor.

Call: “CFC” menu

Requirement: A page-oriented CFC editor is active.

Dialog: Edit Page Size

Elements outside of the workspace are marked in red.

“Width”

Width of the page (minimum 24, maximum 1024)

“Height”

Height of the page (minimum 24, maximum 1024)

“Margin width”

Width of margin column (minimum 6, maximum 25% or page width)

“Set as default for new CFC objects”

_cds_icon_option_activated_copy.png: The current settings are applied as default for new CFC objects.