Symbol:
Function: The command creates a control point at a connector.
Call: “SVN” in the context menu
Requirement: A CFC editor is active. The cursor is located over a connection.
The control point is created at the position on the connecting line where the cursor is located when the command is executed.
Alternatively, you could also drag a control point from the “ToolBox” view to the editor.