Symbol:
Function: The command opens the “Breakpoints” view.
Call: “View” menu
The view shows an overview of all defined breakpoints for an application. You have access to all breakpoint commands within the view.
|
“Application” |
Select the required application from the list. |
|
“POU” |
Name of the POU which will get the breakpoint |
|
“Position” |
Location of the breakpoint in the POU
"(Impl)" indicates that the breakpoint is located in the implementation of the function block, not in an instance. |
|
“Instance Path” |
Full object path of the breakpoint location |
|
“Tasks” |
Names of tasks which should become effective when the breakpoint is executed If there are no restrictions, then "(all)" is displayed here. |
|
“Condition” |
|
|
“Hit Count Condition” |
Specifies when the breakpoint should become effective (depending on the hit count) |
|
“Current Hit Count” |
Specifies how often the breakpoint has already been reached up to now during the execution ("hit") |
|
“Watched Values Last Updated” |
Displays the time of the last update of the watched values |
|
|
The command opens the “Breakpoint Properties” dialog. |
|
|
|
The command opens the “Breakpoint Properties” dialog. |
|
|
“Clear breakpoint” |
Removes the breakpoint Do not confuse this with disabling. |
|
|
“Enable/disable breakpoint” |
Toggles the status of the breakpoint or execution point between "enabled" and "disabled"
Different from “Clear Breakpoint”, a disabled breakpoint remains in the list and can be enabled again. |
|
|
“Properties” |
The “Breakpoint Properties” dialog opens for editing the breakpoint parameters. The dialog corresponds to the “New Breakpoint” dialog. In online mode, you can convert the breakpoint into an execution point. |
|
|
“Go to source position” |
Opens the online view of the relevant POU The cursor is set at the breakpoint location. |
|
|
“Clear all breakpoints” |
Deletes all breakpoints and execution points in the application The list is cleared. Do not confuse this with disabling. |
|
|
“Enable all breakpoints” |
Enables all breakpoints and execution points which are currently disabled |
|
|
“Disable all breakpoints” |
Disables all breakpoints and execution points which are currently enabled The points remain in the list and can be enabled again. |
For more information, see: ⮫ “Using Breakpoints ”



: The breakpoint is disabled.
: The execution point is enabled.
: The execution point is disabled.
: The data breakpoint is disabled.
: The data execution point is enabled.
: The data execution point is disabled.