Dialog 'Options' – 'Multi download tool'Permalink

Symbol: IC_2024_AB_Tools_Multi_download_tool

Function: The multi download tool for AC500 V3 PLCs in Automation Builder enables firmware updates and application downloads of the same project to several PLCs of the same type

Call: Menu bar: “Tools  Options”; category “Multi download tool”.

'Network scan settings'

“Network scan timeout (seconds)”

Maximum time to wait for the network scan results (by default 10 seconds).

“Blink timeout (seconds)”

Maximum time to wait for the blink operation to execute (by default 10 seconds).

'Multi download settings'

“Number of parallel downloads”

How many PLC downloads are executed in parallel (by default 10).

“Download timeout (minutes)”

Name and location of the library that is to be integrated in the project after the conversion.

Depending on the network infrastructure the download might run into errors due to timeouts. The user will not be informed about these timeouts directly, but each timeout might result in errors. To avoid these timeouts the corresponding value can be adapted here in minutes (by default 5 minutes).