SRPermalink

Provided by standard library.

Making bistable function blocks dominant:

Q1 = SR (SET1, RESET) means:

Q1 = (NOT RESET AND Q1) OR SET1

The input variables SET1 and RESET as well as the output variable Q1 are type BOOL.

Declaration example

SRInst : SR ;

Example in Function Block Diagram

COD_SR

Example in Structured Text

SRInst(SET1:= VarBOOL1 , RESET:=VarBOOL2 );

VarBOOL3 := SRInst.Q1 ;