You can use the user-defined reference data type to create an alternative name for a variable, constant or function block.
Create your references as objects in the Object Organizer under the register card “Data types”. They begin with the keyword TYPE and end with END_TYPE.
Syntax:
TYPE <Identifier>: <Assignment term>; END_TYPE
Example:
TYPE message:STRING[50]; END_TYPE;