You are offered a special dialog for setting communication parameters when the communication between the local PC and the runtime system is running over a gateway server in your system. (If the OPC or DDE server is used, the same communications parameters must be entered in its configuration).