SysEthernetPortConfigAndStatus (STRUCT)

TYPE SysEthernetPortConfigAndStatus : STRUCT

Structure containing the Ethernet port configuration and status

InOut:

Name

Type

Comment

udiStructSize

UDINT

Size of the structure SysEthernetPortConfigAndStatus returned from external implementation

udiVersion

UDINT

Version number of the structure

udiMauType

UDINT

Media Access Unit (MAU) type, see MauType constants SYSETH_MAUTYPE_…

uiOperStatus

UINT

Link state of Ethernet port, see OperStatus constants SYSETH_OPERSTAT_…

usiAutoNegSupport

USINT

Auto-negotiation support of MAU, see AutoNegSupport constants SYSETH_AUTONEGSUP_…

usiAutoNegMode

USINT

Auto-negotiation mode of MAU, see AutoNegMode constants SYSETH_AUTONEGMODE_…

uliAutoNegSupportedCap

ULINT

Supported auto-negotiation capabilities of MAU, see AutoNegCaps constants SYSETH_AUTONEGCAP_…

uliAutoNegAdvertisedCap

ULINT

Advertised auto-negotiation capabilities of MAU, see AutoNegCaps constants SYSETH_AUTONEGCAP_…