SysEthernetSetAutoNegAdvertisedCap (FUN)

FUNCTION SysEthernetSetAutoNegAdvertisedCap : SysTypes.RTS_IEC_RESULT

Set advertised auto-negotiation capabilities for an adapter identified by its MAC address.

InOut:

Scope

Name

Type

Comment

Return

SysEthernetSetAutoNegAdvertisedCap

SysTypes.RTS_IEC_RESULT

Runtime system error code (see CmpErrors.library).

Input

macAddress

ARRAY [0..5] OF BYTE

MAC address of the adapter

uliAutoNegAdvertisedCap

ULINT

Advertised auto-negotiation capabilities of MAU, see AutoNegCaps constants SYSETH_AUTONEGCAP_…