PackArrayOfBoolToArrayOfByte (FUN)

FUNCTION PackArrayOfBoolToArrayOfByte : UINT

The function packs an “ARRAY OF BOOL” into an “ARRAY OF BYTE”.

axSource[0] -> abyDestination[0].0
axSource[1] -> abyDestination[0].1
…
axSource[8] -> abyDestination[1].0
…
axSource[15] -> abyDestination[1].7
…

The function copies “uiNumberOfBits” from “axSource” to “abyDestination”. It will return the necessary number of bytes in “abyDestination”. Only if “paxSource”, “pabyDestination” or “uiNumberOfBits” are set to “0”, the copying will not be carried out and the function will return “0”.

Example:

axSource : ARRAY[0..9] OF BOOL := FALSE,TRUE,FALSE,FALSE,TRUE,TRUE,FALSE,FALSE,TRUE,FALSE ;
abyDestination : ARRAY[0..2] OF BYTE ;
uiNumberofBytes := MEM.PackArrayOfBool(ADR(abSource), ADR(abyDestination), 10) ;
->
uiNumberofBytes = 2
abyDestination[0] = 16#32
abyDestination[1] = 16#01
abyDestination[2] = 16#00

Note

The size of the ARRAY “abyDestination” has to be adjusted to the amount of bits copied! Source and target may not overlap!

InOut:

Scope

Name

Type

Comment

Return

PackArrayOfBoolToArrayOfByte

UINT

functon returns the necessary number of bytes in “abyDestination”

Input

paxSource

POINTER TO BYTE

address of ARRAY OF BOOL

pabyDestination

POINTER TO BYTE

address of ARRAY OF BYTE

uiNumberOfBits

UINT

number of bits to copy from “paxSource” to “pabyDestination”