GetTime (FB; Prefix filgt)

FUNCTION_BLOCK GetTime EXTENDS CBM.ETrig

This function block returns date and time of the last modification of the file specified by “sFileName“

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts
Falling edge: Resets outputs
If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrig

Output

xDone

BOOL

TRUE: Action successfully completed

ETrig

xBusy

BOOL

TRUE: Function block active

ETrig

xError

BOOL

TRUE: Error occurred, function block aborts action
FALSE: No error

ETrig

Input

sFileName

CAA.FILENAME

File name

Output

eError

ERROR

Local library error ID (0: no error; 5101: time out)

dtLastModification

DT

Date and time of last modification, for example dt#2006-05-08-00:00:00