SgxWindowMonitoring (FB)
FUNCTION_BLOCK SgxWindowMonitoring EXTENDS AbbLConC3
The “SgxWindowMonitoring” function block detects an returns the maximum and minimum force during measurement
Captures the maximum and minimum value in 16-bit data format within the monitoring cycle
Digital output (DO) indicates the event of “UpperLimit” or “UpperLimit” is reached when it is configured as “Event - application FB”
“Application” determines whether the “UpperLimit” and “LowerLimit” are sourced from channel parameters(Application = FALSE) or functionblock itself (Application = TRUE)
When the digital output is configured as “Event-application FB”, it signals the exceedance OF either “UpperLimit” OR ”LowerLimt”
Monitoring triggers on the Enable = TRUE
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
EnableBOOLFALSE
A rising edge (Enable = TRUE) starts the operation, the output Busy goes to TRUE. All other inputs are read and considered continuously. Execution will continue forever until a falling edge (Enable = FALSE) aborts the operation. During Aborting the Busy is still TRUE. Afterward all outputs are reset.
AbbLConC3
Output
BusyBOOLFALSE
Operation is running (while output Error is FALSE)
AbbLConC3
ErrorBOOLFALSE
Operation is stopped with error (while output Busy is FALSE). This output is TRUE for at least one cycle or until Enable is set to FALSE. The output ErrorID gives more details about the error.
AbbLConC3
Input
PauseBOOLFALSE
0 => Normal operation; 1 => pause the current operation
LockBOOLFALSE
FALSE => continue monitoring; TRUE => lock the current result not to be overlapped
EventOutputEnableBOOLFALSE
FALSE => mask the digital output not to be activated by event; TRUE => enable the event trigger of digital output
DigitalOutputBOOLFALSE
Imaged digital output field when “general digital output” is configured
ObjectSgx_WEIGHT_OBJECT.Net
0 => Net; 1 => Gross
ChannelPOINTER TO SgxChannelIo
Instance of strain gauge channel to be connected
Output
ActiveBOOLFALSE
0 => IndexReturn, MaxValueReturn and MinValueReturn are in progress; 1 => IndexReturn, MaxValueReturn and MinValueReturn are refreshed
ErrorIDERROR_ID.NO_ERROR
Error code returned
OverRunBOOLFALSE
0 => Data read in time; 1 => Data missing (IndexReturn > Previous IndexReturn + 1)
StateReturnWORD0
State of monitoring cycle returned, [0] => digital output state;[1] => ACTIVE; [2] => STATE OF LOCK, [3] = STATE OF EVENT_OUTPUT_ENABLE;[4:7] => Object, 0 = Net, 1 = Gross; [8:9] => fixed unit = 0; [10:11] => diagnosis class; [12:15] => fixed function code = 5
IndexReturnWORD0
Index of monitoring cycle returned
MaxValueReturnINT0
Maximum value of monitoring cycle returned
MinValueReturnINT0
Minimum value of monitoring cycle returned