ERROR_ID (ENUM)

TYPE ERROR_ID

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_ERROR

16#0

No error

ERR_VALUE_INVALID

16#1

At least one field of the value is not supported

ERR_VALUE_TOO_LOW

16#2

Value is less than “LowerLimit” of weight specified

ERR_VALUE_TOO_HIGH

16#3

Value is greater than “UpperLimit” of weight specified

ERR_PARAMETER_ERROR

16#4

Value of parameter is invalid or not supported by module

ERR_FUNCTION_CODE

16#5

Function code is not supported by module

ERR_FAILURE

16#6

Failure to obtain the measurement

ERR_OVERRUN

16#7

The previous value is overwritten by new measurement before fetching when ower sampling rate is faster than cycletime of task

ERR_OCCUPY_CHANNEL

16#8

The same strain gauge input channel has been called and executed by function block

ERR_EXCITATION

16#9

Excitation malfunction

ERROR_WRONG_ADDRESS

16#A

Invalid channel address, the address must not be 0

ERR_BROKEN_WIRE

16#80

Broken wire of external connection

ERROR_SHORT_CIRCUIT

16#81

Short circuit of external connection

ERR_CHANNEL_OVERFLOW

16#82

Overflow of input signal

ERROR_CHANNEL_UNDERFLOW

16#83

Underflow of input signal

ERR_LOW_VOLTAGE

16#84

Voltage is too low to operate

ERROR_PARAMETER_RANGE

16#85

Invalid parameter, value is out of the range specified

ERR_PARAMETER_CRC

16#86

Invalid parameter block due to CRC error detected

ERROR_HARDWARE_ADC

16#87

ADC hardware malfunction

ERR_HARDWARE_REFERENCE

16#88

Internal reference voltage malfunction

ERROR_HARDWARE_COMMUNICATION

16#89

Internal communication error