GetLanguageText (FUN)
FUNCTION GetLanguageText : ReturnValues
This function returns the language specific text of a textlist as STRING.
Note
The desired language must be loaded with CmpDynamicText.DynamicTextLoadLanguage(sLanguage) before the function GetLanguageText is called. For performance reasons, the language should not be loaded/unloaded cyclically. The best way is to load the language after the application has been initialized or when a language change is necessary. The language should be unloaded with CmpDynamicText.DynamicTextUnloadLanguage(sLanguage) when the language texts are not needed anymore.
- InOut:
Scope
Name
Type
Comment
Return
GetLanguageTextPossible last error values:
see ReturnValues (GVL) where possible error reasons are described.
Inout Const
sTextListSTRINGThe textlist name
sTextIndexSTRINGThe textlist id
sLanguageSTRINGIn which language the text should be returned
Input
psTextPOINTER TO STRING
The buffer where the result text should be returned
diSizeDINTThe size of the parameter psText in byte (SIZEOF() can be used)
Output
bDefaultTextBOOLIndicates if the default text is used