MemoryManager (FB)
FUNCTION_BLOCK PUBLIC MemoryManager
The MemoryManager maintains a mbm message exchange. If the last message was taken from the exchange, it automatically extends the exchange by the actual size. This can be disabled by setting AutoExtend = FALSE.
How to use:
Call Create() with the block size and the number of blocks you would like to pre-allocate.
Call Malloc() whenever you need memory. As long as MessagesLeft > 0 OR AutoExtend = FALSE, no SysMemAlloc will be performed!
Call Free() to free memory allocated at the MemoryManager.
Call Delete() before shutting down the system.
Properties:
ActSize
AutoExtend
Exchange
InitSize
MessagesLeft
Methods:
Create
Delete
FB_Exit
Free
Malloc
Structure: