SerializeHexReal (FUN)

FUNCTION SerializeHexReal : STRING(32)

Converts a floating point number to the format
F16#{Mantissa}H{Exponent}
where both mantissa and exponent are hexadecimal numerals, such that liM * 2^iE = {Mantissa} * 16^{Exponent}.

Note

  • If liM is zero, {Exponent} is set to 0, regardless of the value of iE.

  • The hexadecimal exponent is computed as floor(iE/4). The hexadecimal mantissa then becomes liM * 2^(iE mod 4).

See also DeSerializeHexReal.

InOut:

Scope

Name

Type

Comment

Return

SerializeHexReal

STRING(32)

Input

liM

LINT

The (signed) mantissa

iE

INT

The (unbiased) exponent