ITypeDescWithReferenceType (ITF)

INTERFACE ITypeDescWithReferenceType EXTENDS ITypeDesc

TypeDesc nodes which have a base type implement this interfaces. This can be used for the TypeDesc nodes of derived FBs, as well as e. G. for alias types or subrange types.

Methods:

GetReferenceBaseType

FindNode, inherited from ITypeDesc

Get, inherited from ITypeDesc

GetNativeSize, inherited from ITypeDesc

GetSize, inherited from ITypeDesc

GetSize2, inherited from ITypeDesc

GetSwapSize, inherited from ITypeDesc

GetTypeClass, inherited from ITypeDesc

GetTypeDesc, inherited from ITypeDesc

GetTypeNode, inherited from ITypeDesc

NodeFound, inherited from ITypeDesc

Set, inherited from ITypeDesc

Swap, inherited from ITypeDesc

Swap2, inherited from ITypeDesc

Structure: