Analyzation (LIB)

Version

4.1.0.0

Namespace

Analyzation

Author

3S-Smart Software Solutions

Placeholder

Analyzation

Description 1

Analysis of expressions with the Analyzation library

This library provides modules for the analysis of expressions. If a composed expression is FALSE, those of its components can be evaluated which are adding to this result. In the SFC-Editor the flag SFCErrorAnalyzationTable uses this function implicitely for the analysis of expressions in transitions.

Example of an expression:

b OR NOT(y < x) OR NOT (NOT d AND e)

The functions:

The following variables are used by all modules:

InputExpr: BOOL, expression to be analysed

DoAnalyze: BOOL, TRUE starts analysis

ExpResult: BOOL, current value of the expression

Result of the analyzation:

AnalyzeExpression returns in a string the components of the expression, which are adding to the total value FALSE.

OutString: STRING, Result of the analysis, Sequence of the concerned components of the expression (e.g. y < x | d)

AnalyseExpressionTable writes the components of the expression, which are adding to the total value FALSE, to an array. For each component the following information is provided by structure ExpressionResult: name, address, comment, (current)value.

OutTable: ARRAY [0..15] OF ExpressionResult;

e.g..

CODESYS - Intern/SFC/Images/sfc_settings.png

Figure 1: SFC settings

CODESYS - Intern/SFC/Images/sfc_analyzation.png

Figure 2: SFC analyzation example

AnalyseExpressionCombined combines the functionalities of AnalyzeExpression plus AnalyseExpressionTable

Contents:

Indices and tables

1
Based on Analyzation.library, last modified 28.10.2021, 08:36:40. LibDoc 4.6.0.0-r.29
The content file Analyzation.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 28.10.2021, 08:36:41.