UDPDriver.Select (METH)
METHOD Select : SysTypes.RTS_IEC_RESULT
Encapsulates SysSockSelect.
- InOut:
Scope
Name
Type
Comment
Return
SelectSysTypes.RTS_IEC_RESULTInput
iTimeOutINTTime out in micro seconds, set to 0 to disable time out.
Inout
strRecvSetSysSocket.SOCKET_FD_SETList of streams to be checked for receive. Only streams which are ready for reception will remain in this list.
strSendSetSysSocket.SOCKET_FD_SETList of streams to be checked for send. Only streams which are ready for sending will remain in this list.
strErrorSetSysSocket.SOCKET_FD_SETList of streams to be checked for errors. Only streams which are having an error will remain in this list.
Output
diReadyDINTeLogCodeErrorCode