IRPCCLClient.Abort (METH)

METHOD Abort : ERROR

This method should be called if the Client is in CommFail or Fault state. It aborts all Client operations immediately without notifying the server. CARE: During a pending request the Cancel-Method should be used to terminate the request first!

InOut:

Scope

Name

Type

Return

Abort

ERROR