ListFactory.CreateDynamicList (METH)

METHOD FINAL CreateDynamicList : IList2

Creates a dynamic list. Note: Function blocks which are created with this factory are NOT online change safe.

InOut:

Scope

Name

Type

Comment

Return

CreateDynamicList

IList2

Input

udiInitialSize

UDINT

Initial size of elements. Must not be 0.

uiGrowFactor

UINT

Grow factor for dynamic memory reallocation if the number of elements is greater than udiInitialSize. Use 1 to disable dynamic memory reallocation.

Output

eError

FBF.ERROR