HashTableFactory.CreateDynamicHashtable (METH)
METHOD FINAL CreateDynamicHashtable : IMap2
Creates a dynamic hashtable. Note: Function blocks which are created with this factory are NOT online change safe.
- InOut:
Scope
Name
Type
Comment
Return
CreateDynamicHashtableInput
udiInitialSizeUDINTInitial size of elements. Must not be 0.
uiGrowFactorUINTGrow factor for dynamic memory reallocation if the number of elements is greater than udiInitialSize. Use 1 to disable dynamic memory reallocation.
Output
eErrorFBF.ERROR