CANopenManager_Diag.SetCommunicationState (METH)
METHOD SetCommunicationState : DED.ERROR
Starts, stops or resets the device. Following table defines the mapping between CAA Device Diagnosis
DED.DEVICE_TRANSITION_STATE and CANopen NMT command:
CAA Device Diagnosis |
CANopen NMT command |
|
NMT Start |
|
NMT Stop |
|
NMT Reset; leads to reset of all slaves |
Note
Use CANopenManager_Diag.CheckCurrentSupportedCommunicationState to check which transitions are possible in the current state!
- InOut:
Scope
Name
Type
Comment
Return
SetCommunicationStateDED.ERRORDED.ERROR.NO_ERRORif device transition was successful.Input
eRequestedStateDED.DEVICE_TRANSITION_STATEdesired transition