CANRemoteDevice_Diag.CheckCurrentSupportedCommunicationState (METH)

METHOD CheckCurrentSupportedCommunicationState : BOOL

This method checks if a specific DED.DEVICE_TRANSITION_STATE can be processed in the current state.
For more details on interpretation of DED.DEVICE_TRANSITION_STATE for CANopen see CANRemoteDevice_Diag.SetCommunicationState.

Note

Use CANRemoteDevice_Diag.CheckSupportedCommunicationState to check which DED.DEVICE_TRANSITION_STATE is supported in general.

InOut:

Scope

Name

Type

Comment

Return

CheckCurrentSupportedCommunicationState

BOOL

TRUE if node supports the requested DED.DEVICE_TRANSITION_STATE in the current state.

Input

eRequestedState

DED.DEVICE_TRANSITION_STATE

The communication state to be checked.