Derivative (FB)
FUNCTION_BLOCK Derivative
This function block will approximate the first derivative \(f\prime\) of a function \(f = f(t)\) at the actual time \(t_{n}\) with the respect to the values of the last three function calls according to the BDF method:
\[f\prime (t_{n}) \doteq \frac{3 (f(t_{n}) - f(t_{n-3})) + f(t_{n-1}) - f(t_{n-2})}{3(t_{n-2}-t_{n-3})+4(t_{n-1}-t_{n-2})+3(t_{n}-t_{n-1})}\]
- InOut:
Scope
Name
Type
Comment
Input
xEnableBOOLreset
lrInputValueLREALactual function value
udiTMUDINTlength of time interval \([t_{n-1}, t_{n}]\) (equals time passed since last call to function)
Output
lrDerivativeLREALapproxmated value of first derivative
xValidBOOLValidity of resultFALSE: If the number of calls neccessary for approximating has not been executed yet.