TCP_Connection (FB)

FUNCTION_BLOCK TCP_Connection EXTENDS CBM.LTrig

The next free connection is determined by handle exchange and set to active. As long as xActive is TRUE the handle of the connection is valid. If xActiveis FALSE the handle of the connection is invalid. hConnection can be used as input hConnection for function blocks TCP_Write, TCP_WriteBuffer, TCP_Read and TCP_ReadBuffer.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xEnable

BOOL

TRUE: Action starts
FALSE: Action stops, outputs xDone, xBusy, xError are resetted

LTrig

Output

xDone

BOOL

TRUE: Action successfully completed

LTrig

xBusy

BOOL

TRUE: Function block active

LTrig

xError

BOOL

TRUE: Error occurred, function block aborts action
FALSE: No error

LTrig

Input

hServer

CAA.HANDLE

Output

eError

ERROR

xActive

BOOL

hConnection

CAA.HANDLE

Properties:

IPAddress

Structure: