FactoryBase (FB)
FUNCTION_BLOCK FactoryBase IMPLEMENTS IFactory
This function block implements the neccecary basic functionality for a function block factory.
Memory allocator
AllocInstMem
FreeInstMem
The allocator use the following properies as parameters.
InstSize reports the memory consumtion of the related function block instance.
InstPoolAdr, InstPoolSize => The instance pool is initialized with a static memory area.
InstCout, InstPoolSize => The instance pool is initilaized with a memory area from the heap.
InstPoolExtendsFactor => The instance pool can be extended dynamically with memeory areas from the heap.
List management for handling the group of produces function block instances.
InsertInst
RemoveInst
Properties:
prvInstCount
prvInstPoolAdr
prvInstPoolExtendsFactor
prvInstPoolSize
prvInstSize
Methods:
FB_EXIT
FB_INIT
prvInstInit
Structure: