PERSISTENT_PDATA_HEADER (STRUCT)
TYPE PERSISTENT_PDATA_HEADER : STRUCT
structure which contains PERSISTENT data header information for each object as header in the data file…
- InOut:
Name
Type
Comment
magicCodeUDINTshould be PDATA_HEADER_MAGIC
versionWORDversion field for future use
headerSizeWORDsize of the header structure
entrySizeWORDsize of (W_PDATA_ENTRY)
objectIDCmpBACnet.IEC_BACNET_OBJECT_IDthe object ID
deviceIdCmpBACnet.IEC_BACNET_UNSIGNEDdevice of object
clientCreatedBOOLwas client created object