LogObjectsBase (FB)

FUNCTION_BLOCK ABSTRACT LogObjectsBase EXTENDS BACnet.BACnetServerPluginBase

Base class for logging objects default implementions (Trend_Log, Trend_Log_Multiple, Event_Log). It tries to provide a feature complete implementation for logging objects with a reasonable simple implementation.

Assumptions / provisions of LogObjectBase and derived: A.) All log data are stored in the file system, one file per object.

If large data volumes should be used (Buffer_Size) a high performance file system is recommended.

B.) no sophisticated Sequence / Total_Record_Count overflow handling needed - they simply overflow / wrap around

If those assumptions / provisions are not valid for your use case, a more sophisticated implementation is needed, for example based on database, in-memory-database etc.

BACstack log data are delivered as either IEC_BACNET_LOG_RECORD, IEC_BACNET_LOG_RECORD_MULTIPLE, or IEC_BACNET_EVENT_LOG_RECORD packed in a IEC_BACNET_PROPERTY_CONTENTS and are stored binary as is in one file per logging object.

Such a log file contains: 1.) file header 2.) 0..numRecords-1 log records

A log record in such a file consists of: 1.) log record header

  • sequence : IEC_BACNET_UNSIGNED

  • time stamp : IEC_BACNET_DATE_TIME

2.) log record data as C-structure 3.) actual number of records in file : IEC_BACNET_UNSIGNED

Reasons to do so: - SysFile write operations in append mode doesnt allow writing at file pos <> end for some platforms - reading the last record should be efficient (rewind from file end), for example to get last sequence number

If the number of records is supposed to be limited practically (Buffer_Size), then purge operations of the data files are needed (to get rid of old records). Those purge operations are done implicitely in the implementation. A purge operation basically copies the records - except the purged record(s) - to a temporary file, deletes the data file, copy/move the data file to the data file. For those purge operations it might be useful to choose a TempPath on a high speed file system (RAM file system). If TempPath <> PersistentPath the temporary file will be copied to the data file and deleted afterwards, otherwise the temporary file will be renamed to the data file.

The purge operations involve a significant performance degradation. In general this should not be an issue, because BACnet logging objects are designed to inform a BACnet management device (OWS/AWS) about “log buffer mostly full” via Notification_Threshold and notifications. The BACnet management device should read and clear the log buffer to avoid “log buffer full” situations which will cause loss of logging data anyway.

Properties:

HardShutdown

MaxDataSize

ObjectType

PersistentPath

ServerDeviceId

TempPath

Methods:

FreeReadRangeResult

GetBufferSize

GetRecordsByPosition

GetRecordsBySequence

GetRecordsByTime

GetStopWhenFull

Init

PostStopBACnetStack

ReadRangeResultSetInfo

ScanObjectsAndSetCallbackAttachments

SetCallbackAttachments

SetReadCallbackAttachment

SetWriteCallbackAttachment

UpdateObjectPropertiesFromDataFile

ComputeRecordSize

CreateDataFiles

DataFileName

ListDataFiles

LogDataFile

LogFilePos

LogFileSize

LogFileSizeAndPos

LogObjectAddrString

LogObjectPropertyAddrString

LogReadRangeResult

LogRecord

LogRecordContentInfo

ObjectId

PurgeDataFile

ReadNumberOfRecordsAndLastSequenceFromDataFile

ReadNumberOfRecordsFromDataFile

ReadRangeErrorCompletion

ReadRangeInfoToString

RemoveDataFiles

RemoveUnusedDataFiles

ResetDataFile

WriteRecordContentToDataFile

Structure: