InitializeEmptyPropertyInstance (FUN)

FUNCTION InitializeEmptyPropertyInstance : BOOL

Initializes a property (prop) with its (working) defaults (mostly empty) considering constant array sizes, lists and special property types.

InOut:

Scope

Name

Type

Comment

Return

InitializeEmptyPropertyInstance

BOOL

Input

objTyp

CmpBACnet.IEC_BACNET_OBJECT_TYPE

The object instance which has the desired property.

accessID

CmpBACnet.IEC_BACNET_ACCESS

The access specifier used for initializing the property instance.

propID

CmpBACnet.IEC_BACNET_PROPERTY_ID

The property ID of the property for which the instance data shall be initialized.

Inout

prop

CmpBACnet.IEC_BACNET_PROPERTY_INSTANCE