BACnetSchedule.AddPropertyReference (METH)
METHOD AddPropertyReference : CmpBACnet.IEC_BACNET_STATUS
Adds device object property reference to the List_Of-Object_Property_References-Property (which lists all the Objects to influenced by this Schedule) of this BACnet-Object.
- InOut:
Scope
Name
Type
Initial
Comment
Return
AddPropertyReferenceCmpBACnet.IEC_BACNET_STATUSInput
deviceInstanceCmpBACnet.IEC_BACNET_DWORDThe BACnet device to reference.
objInstanceCmpBACnet.IEC_BACNET_DWORDThe BACnet object instance number of the BACnet device to reference.
objTypeCmpBACnet.IEC_BACNET_OBJECT_TYPEThe BACnet object type number of the BACnet device to reference.
propIDCmpBACnet.IEC_BACNET_PROPERTY_IDThe BACnet property ID of the BACnet object to reference.
nIndexCmpBACnet.IEC_BACNET_SIGNEDThe 1 based index to reference of the BACnet property.
xDevicePresentBOOLTRUE
Whether the BACnet device is present or not.