BACnetIntegerValue.GetPriorityArray (METH)
METHOD GetPriorityArray : CmpBACnet.IEC_BACNET_STATUS
Gets the Priority-Array of this BACnet object. The returned pointer pPrioArray is allocated with the corresponding data, whereas the user has to use FreeStackAllocatedMemory, to free the allocated memory after data usage.
- InOut:
Scope
Name
Type
Comment
Return
GetPriorityArrayCmpBACnet.IEC_BACNET_STATUSOutput
pPrioArrayPOINTER TO ARRAY [1..16] OF CmpBACnet.IEC_BACNET_PRIORITY_ARRAY_ITEM
The returned Pointer gets filled with the data of the Priority Array AND (!) the data referenced within the array (i.e. strings, etc.). After usage, use FreeStackAllocatedMemory, to free the used memory again.