BACnetGroup.GetListOfGroupMembers (METH)
METHOD GetListOfGroupMembers : CmpBACnet.IEC_BACNET_STATUS
Gets the List_Of_Group_Members of this BACnet object. The returned pointer is allocated with the corresponding data, whereas the user has to use FreeStackAllocatedMemory, to free the allocated memory after data usage.
- InOut:
Scope
Name
Type
Comment
Return
GetListOfGroupMembersCmpBACnet.IEC_BACNET_STATUSOutput
uiListCountCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe length of the list in the following pointer
pListPOINTER TO CmpBACnet.IEC_BACNET_READ_ACCESS_SPEC
The returned Pointer gets filled with the data of the List AND (!) the data referenced within that list (i.e. strings, etc.). After usage, use FreeStackAllocatedMemory, to free the used memory.