BACnetDevice.GetVTClassesSupported (METH)
METHOD GetVTClassesSupported : CmpBACnet.IEC_BACNET_STATUS
Gets the VT_Classes_Supported-List of this BACnet object. The returned pointer is allocated with the corresponding data, whereas the user has to use FreeStackAllocatedMemory, to free the allocated memory after data usage.
- InOut:
Scope
Name
Type
Comment
Return
GetVTClassesSupportedCmpBACnet.IEC_BACNET_STATUSOutput
uiListCountCmpBACnet.IEC_BACNET_ELEMENT_COUNTThe length of the list in the following pointer*)
pListPOINTER TO CmpBACnet.IEC_BACNET_VT_CLASS
The returned Pointer gets filled with the data of the List AND (!) the data referenced within that list (i.e. strings, etc.). After usage, use FreeStackAllocatedMemory, to free the used memory again.