BACnetAnalogOutput.WritePresentValueNullWithPriority (METH)
METHOD WritePresentValueNullWithPriority : CmpBACnet.IEC_BACNET_STATUS
Set the Present_Value to NULL with the given priority taking client side restrictions into account (access, priorization, range checks). In contrast to SetPropertyInstance and |PresentValue.Set| all access, priorization and range checks are executed by this call and on return the occurred BACnet error code will be returned.
- InOut:
Scope
Name
Type
Comment
Return
WritePresentValueNullWithPriorityCmpBACnet.IEC_BACNET_STATUSInput
priorityDINTThe priority to use when writing to Present_Value.