BACnetAccumulator (FB)

FUNCTION_BLOCK PUBLIC BACnetAccumulator EXTENDS BACnetStaticObjectBase IMPLEMENTS IBACnetAccumulator

FB reflecting a BACnet-Accumulator-Object. All Properties of this FB give access to the client writeable BACnet-Properties of the reflected BACnet-Object, although the access is done not client sided (without checking access restrictions). Additionaly access is given for the Present_Value-Property, although the latter is not (always) client side writeable. Moreover access right behaviour which changes due to dynamically changing BACnet-Property-Sets is done by an Event-Callback (BACnetEventCallback), which is attached to the BACNET_CALLBACK_WRITE-Callback. Additionally see documentation of BACnetObjectBase.

Properties:

AckedTransitions

Description

DeviceType

EventAlgorithmInhibit

EventAlgorithmInhibitRef

EventDetectionEnable

EventEnable

EventMessageTexts

EventMessageTextsConfig

EventState

EventTimeStamps

HighLimit

LimitEnable

LimitMonitoringInterval

LoggingObject

LoggingRecord

LowLimit

MaxPresValue

NotificationClass

NotifyType

OutOfService

Prescale

PresentValue

ProfileName

PulseRate

Reliability

ReliabilityEvaluationInhibit

Scale

StatusFlags

TimeDelay

TimeDelayNormal

Units

ValueBeforeChange

ValueChangeTime

ValueSet

NumberOfProperties, inherited from BACnetObjectBase

ObjectID, inherited from BACnetObjectBase

Methods:

GetBACnetAccumulatorRecordProperty, inherited from BACnetObjectBase

GetBACnetArraySizeOfProperty, inherited from BACnetObjectBase

GetBACnetArraySizeOfTwoProperties, inherited from BACnetObjectBase

GetBACnetBitStringProperty, inherited from BACnetObjectBase

GetBACnetBooleanProperty, inherited from BACnetObjectBase

GetBACnetClientCOVProperty, inherited from BACnetObjectBase

GetBACnetDateProperty, inherited from BACnetObjectBase

GetBACnetDateRangeProperty, inherited from BACnetObjectBase

GetBACnetDateTimeProperty, inherited from BACnetObjectBase

GetBACnetDevObjPropReferenceProperty, inherited from BACnetObjectBase

GetBACnetDoubleProperty, inherited from BACnetObjectBase

GetBACnetEnumeratedProperty, inherited from BACnetObjectBase

GetBACnetObjPropReferenceProperty, inherited from BACnetObjectBase

GetBACnetObjectIDProperty, inherited from BACnetObjectBase

GetBACnetPrescaleProperty, inherited from BACnetObjectBase

GetBACnetRealProperty, inherited from BACnetObjectBase

GetBACnetScaleProperty, inherited from BACnetObjectBase

GetBACnetSetpointReferenceProperty, inherited from BACnetObjectBase

GetBACnetSignedProperty, inherited from BACnetObjectBase

GetBACnetStringProperty, inherited from BACnetObjectBase

GetBACnetTimeProperty, inherited from BACnetObjectBase

GetBACnetTimeStampProperty, inherited from BACnetObjectBase

GetBACnetUnsignedProperty, inherited from BACnetObjectBase

GetPropertyAccessRight, inherited from BACnetObjectBase

GetPropertyCallbackAttachment, inherited from BACnetObjectBase

GetPropertyId, inherited from BACnetObjectBase

GetPropertyInstanceStackAllocContentBuffer, inherited from BACnetObjectBase

GetPropertyInstanceWithContentBuffer, inherited from BACnetObjectBase

IsBACnetDateTimePropertyUnspecified, inherited from BACnetObjectBase

IsPropertyExistent, inherited from BACnetObjectBase

IsPropertyWriteable, inherited from BACnetObjectBase

SetBACnetAccumulatorRecordProperty, inherited from BACnetObjectBase

SetBACnetBitStringProperty, inherited from BACnetObjectBase

SetBACnetBooleanProperty, inherited from BACnetObjectBase

SetBACnetClientCOVProperty, inherited from BACnetObjectBase

SetBACnetDateProperty, inherited from BACnetObjectBase

SetBACnetDateRangeProperty, inherited from BACnetObjectBase

SetBACnetDateTimeProperty, inherited from BACnetObjectBase

SetBACnetDateTimePropertyToUnspecified, inherited from BACnetObjectBase

SetBACnetDevObjPropReferenceProperty, inherited from BACnetObjectBase

SetBACnetDoubleProperty, inherited from BACnetObjectBase

SetBACnetEnumeratedProperty, inherited from BACnetObjectBase

SetBACnetObjPropReferenceProperty, inherited from BACnetObjectBase

SetBACnetObjectIDProperty, inherited from BACnetObjectBase

SetBACnetPrescaleProperty, inherited from BACnetObjectBase

SetBACnetRealProperty, inherited from BACnetObjectBase

SetBACnetScaleProperty, inherited from BACnetObjectBase

SetBACnetSetpointReferenceProperty, inherited from BACnetObjectBase

SetBACnetSignedProperty, inherited from BACnetObjectBase

SetBACnetStringProperty, inherited from BACnetObjectBase

SetBACnetTimeProperty, inherited from BACnetObjectBase

SetBACnetTimeStampProperty, inherited from BACnetObjectBase

SetBACnetUnsignedProperty, inherited from BACnetObjectBase

SetObjectName, inherited from BACnetObjectBase

SetPropertyAccessRight, inherited from BACnetObjectBase

SetPropertyCallbackAttachment, inherited from BACnetObjectBase

SetPropertyInstance, inherited from BACnetObjectBase

WritePropertyInstance, inherited from BACnetObjectBase

Structure: